Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
AmplifierProblem-Slide16

Shown here are symptoms for another common amplifier problem. The circuit illustrated here is used to introduce some DC offset at the output as the engineer can only accommodate positive signals between 0 and 5 V as an example. It is observed that there is much more common mode voltage present at the output much more than the CMRR would be predict. It is as if there is very little or no attenuation of this common mode signal at all from the input to the output. Of course, this wreaks havoc with the subsequent signal conditioning stages of the ADC stage.

PTM Veröffentlicht am: