Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
AS5600 Magnetic Position Sensor Slide 7

Because the AS5600 has an internal LDO, it can be used with 5 V supply or 3.3 V supply. The output update rate and power consumption are determined by the selected power mode. In the fastest mode the current consumption is 6.5 mA and goes down to 1.5 mA, at a 100 ms polling time. Additionally,  there is a feature called watchdog which can be used to automatically switch to the lowest power consumption if there is no activity for one minute.

PTM Veröffentlicht am: