Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
GIG-Array Mezzanine Connectors Slide 3
The FCI Gig-Array connector system is designed as a 100Ώ differential pair system, as is commonly used in high speed signal transmission today. Up to 10Gb performance and low crosstalk assures that the electrical signals will be transmitted cleanly between boards. Mechanical and electrical reliability are achieved by a contact system that provides two points of contact for a signal, and housing polarization features to help prevent plugging the two halves together incorrectly.
PTM Veröffentlicht am: