Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Innovative Current Sensor Packaging Sensing

Shown here are uniquely effective, patented packaging technique for Hall-effect current sensor ICs employed in an SOIC8 flip-chip package. The current to be sensed flows through the conductive copper path between the two pins at the upper left corner of the package and the two pins at the upper right corner of the package. The Hall-effect IC is assembled into the package using standard flip chip assembly techniques. Three major advantages result: First the Hall-effect sensing element is in close proximity to the current-carrying conductor, thereby maximizing magnetic coupling and signal to noise ration that improves device accuracy. Second the Hall-effect IC is not in contact with the integrated conductor, thereby maintaining voltage isolation and enabling working voltages as high as 500 VRMS needed on the DC side of the PV inverter and in line voltage applications. Solder bumps attached to the low-voltage input/output pads on the Hall IC make contact with the lead fingers shown in the upper portion of the right figure. Finally, since the Hall-effect current sensor linear IC is fully integrated it allows Allegro to factory program the device to compensate for zero amp and sensitivity variation over temperature.

PTM Veröffentlicht am: