Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Image of Advantech Growth of AI in Embedded and at Edge - MIC-AI Series of System Video PDF

Advantech would like to introduce the JETSON family of modules. NVIDIA JETSON is designed to enable artificial intelligence at the edge of the network and autonomous systems. The family is made up of four product lines: NANO, TX2 series, and the Xavier series, which includes NX and AGX. Each product line provides modules that combine NVIDIA's embedded GPU system-on-a-chip (SoC) with memory, power management, and multiple I/O interfaces. The family is designed to scale from edge based systems to fully autonomous machines and uses the same software stack so customers can easily leverage the product line across different products or applications. The JETSON NANO is the smallest and lowest power module in the family. It can run all standard frameworks and networks and supports multiple camera and sensor interfaces. The JETSON TX2 series expands on the capabilities found in the NANO and provides three times the performance. The TX2 series has three different SOM variations and these are the TX2 4 GB, the TX2, and the TX2i which is designed and specified for industrial applications. Each module has its own unique specification. Finally, the Xavier series provides the highest level of performance and is capable of running power efficient systems autonomously. There are two modules in the series, the Xavier NX with the same form factor of NANO and the performance of Xavier. Similar to the TX2 series, each module has its own unique specification. Click on this video link to learn more about the Advantech Edge AI Platform, or click to download the selection guide brochure.

PTM Veröffentlicht am: