Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
BLC-Slide5

There is a balance between heat flowing to the board and heat flowing through the case of a BGA, similar to current through a set of resistors in parallel. Decreasing the thermal resistance of the heatsink allows more heat to escape through the heatsink and less injected into the board. This affects the board temperature and the junction temperature of the component itself.

PTM Veröffentlicht am: