Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Slide6
The ATS re-circulating chiller’s front panel display shows water level, pressure, and temperature during operation. The PID controller alerts the system to small temperature fluctuations, which enables fast response time. The system is lightweight and portable, allowing it to easily be moved to the application site. In case of poor ventilation, a safety feature is included that provides automatic shut-off to protect the chiller from over pressure and compressor overload.
PTM Veröffentlicht am: