Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
heat-pipe-slide6

When the evaporator section (Le) is exposed to a heat source, the liquid inside vaporizes and the pressure in that section increases. The increased pressure causes the vapor to flow at a fast speed toward the condenser section of the heat pipe (Lc). The vapor in the condenser section loses heat to the integral heat sink and is converted back to liquid by the transfer of the latent heat of vaporization to the condenser. The liquid is then pumped back to the evaporator through the wick capillary action. The middle section of the heat pipe (La), the adiabatic portion, has a very small temperature difference. This graph shows the pressure drop distribution inside a heat pi pe. In order for the capillary force to drive the vapor, the capillary pressure of the wick should exceed the pressure difference between the vapor and the liquid at the evaporator. This also shows that if the heat pipe is operated against the force of gravity, the liquid undergoes a larger pressure drop. The result is less pumping of the wick with reduced heat transfer. The amount of heat transfer decrease depends on the particular heat pipe.

PTM Veröffentlicht am:
PTM Updated on: 2016-02-05