Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
IDC-Slide11

This magnified ashows the terminated contacts, numbers 2 and 4 and the adjacent conductors in this .100” socket. The contacts terminated to conductors 1, 3 and 5 are offset by .050” and located behind the front row in which contacts 2 and 4 are located. Again, the stranded wire bundles are compressed in the U-slot making a secure, gas tight connection. In this example of a .100” socket, the cable is stranded 28AWG ribbon cable, but the same contact can also accommodate 26AWG stranded or solid wire conductors of the same gauges.

PTM Veröffentlicht am: