Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
3-Phase UPS Systems Slide 5

Redundancy is simply a backup. Network managers deploy redundant servers to ensure continuous data availability. E3 Series 3-Phase UPS Systems deliver redundancy both internally and externally to provide continuous power availability. Redundancy is often referred to in terms of "N", "N+1", "N+2", and many more. In simple terms, "N" is what it needs to get the job done. "N+1" is what it needs to get the job done, plus a little more. Cars provide a common example of N+1 redundancy. Four tires (N) are required to support a standard car; however, one spare tire (+1) is usually included if one of the tires fails or is removed for maintenance. "1+1" redundancy (also known as "N+N") goes one step further. Instead of providing "just a little more" to get the job done, it provides an entire identical system as a backup. Going back to the car as a common example of 1+1 redundancy. One brake system (1) is required to stop a car; however, one emergency brake system (+1) is included if the main system fails.

PTM Published on: 2015-02-04