Maker.io main logo

The Hacksmith: Flame Thrower Exhaust for a Spy Car

38

2018-12-20 | By The Hacksmith

License: See Original Project

This project was created by Engineering Superheroes of Hackmith Industries.

DO NOT ATTEMPT to Re-Create

The latest addition to Hacksmith Industries’ MGB MK4 spy car is “straight fire,” as the kids say these days. This is the fourth spy car feature out of 32 that are planned. Despite having an assortment of gadgets that can shock you or toss you into the air, there wasn’t a feature that can literally melt your face… until now.

Does a spy car need flaming exhaust? Probably not, but a spy needs all the gadgets they can get for a car chase. Worst case scenario, it discourages tailgaters from following too closely. See how it was made in the video below.

 

How Does it Work?

The flames are fueled by a small propane tank that sits in the MK4’s trunk. The propane tank feeds into the car’s exhaust, which propels the flames to shoot a few feet. The flames are triggered by a spark plug at the end of the exhaust. The spark plug is triggered by a solenoid that is controlled by an Arduino. This Arduino controller system is powered by the car’s 12V battery.

The solenoid that toggles the spark plug on and off is controlled via a smartphone app that was developed in a program called Blynk. The app made in Blynk contains the software that controls all of the MK4’s electronic add-ons, including but not limited to the drive in movie projector, the security system, the license plate flipper, and the ejector seat.

More Spy Car Upgrades

Be sure to check out the Hacksmith VLOGs channel if you want to see up to date tests and construction on the spy car. And be sure to check out more spy car projects on Maker.io!

Shocking Security System for a Spy Car

Drive-in Movie Projector

More Vehicle Upgrades with Arduino

Arduino-Controlled Jet Engine for a Motorcycle

Arduino-Controlled LED System for the Bat Baja

Remote Controlling a Baja with an Arduino

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.