This project was created by Engineering Superheroes of Hackmith Industries.
DO NOT ATTEMPT to Re-Create
With a new Batman movie out — this time, featuring Robert Pattinson as “The Batman” — it’s time for another Hacksmith-built Batman project! Hacksmith Industries has made several batarangs, a grapple gun, and a mini batmobile in the past, but no makers have ever attempted to recreate the iconic Bat-signal. One might think this is an easy project: all you need to do is slap a Batman logo on a spotlight… right?
It turns out that projecting an image like the Bat-signal on clouds is much more complicated than initially thought. See how Hacksmith team members Chris and Akshat design their Bat-signal to get around these engineering challenges in the video below!
How Does it Work?
It turns out that light from a typical spotlight doesn’t work the way it does for Bruce Wayne. When you stick a Bat symbol on the glass or plastic that covers a standard spotlight, the symbol will not project because it lacks a lens to project the image. With that in mind, the Hacksmith placed a smaller bat logo (upside down) in front of the LEDs, toward the back of the Bat-signal, and a large focusing lens on the front to project the image into the sky.
The light itself comes from 4 massive LEDs — similar to what was used in the world’s brightest flashlight. These LEDs are so powerful that the Bat-signal needed an industrial water chiller to keep them cool. They also consume a lot of power, so the Bat-signal is hooked up to a gas-powered generator. The spotlight, with all of its components and a sturdy stand to keep it upright, weighs over 1000 pounds and has to be hauled around in a pickup truck!
Check out the schematic of the Hacksmith’s bat signal project below!
Schematic and BOM
More Bright Lights
More Projects from the DC Universe
Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.
Visit TechForumCo-Browse