DC/DC Converters for AI Data Centers: Tackling Space and Thermal Challenges
AI data center GPUs are pushing beyond 1 kW per device resulting in rack power densities in the megawatt scale, stressing cooling schemes past comfort zones.
Webinar – Meet the LAN Squad: Defeating Ethernet Design Challenges
Explore how solutions from Würth Elektronik offer tailored advantages to LAN enhance robustness, simplify layout decisions, and reduce overall system cost.
Measuring the Speed of Sound Using an Ultrasonic Sensor and Oscilloscope
In this blog, I will walk through a simple experiment that uses an ultrasonic sensor and oscilloscope to measure how fast sound travels through the air.
Select the Right Connectors to Meet Stringent Mil/Aero Electrical and Mechanical Requirements
Publish Date: 2026-04-01
Connectors for aerospace and defense integrate sophisticated materials, contact and body design, fabrication, and evaluation to meet mandated objectives.
Single-Chip Systems, MCUs for Matter-Enabled Smart Home Devices Fill Multiple Mesh Network Roles
Publish Date: 2026-03-31
Energy-efficient, low-latency components from NXP support Matter-enabled smart home networks while development tools help designers create new prototypes.
Power Distribution Boards: Smart Alternative to Relays
This blog will talk about the core concepts and the theory behind the circuit schematic and how it was approached.
Harnessing AI at the Edge with iWave’s Agilex™ 5 System on Module
As data processing increasingly moves closer to the edge, platforms that deliver efficient AI performance with low latency and high customization are needed.
Webinar – Seven Reasons to Move from 12 V to 48 V Today
A discussion on why 48 V is becoming the dominant power delivery network and how modular power solutions can speed and simplify transition.
Simplifying Frequency Stability for High-Speed 5G and Data Converter Designs
Publish Date: 2026-03-25
Discover how ADI's ADF4382 PLLs with integrated VCOs enhance frequency stability and speed for high-speed data converter and 5G radio designs.
Building Quantum-Resilient Embedded Systems with iWave’s Agilex™ 5 System on Module
iWave Global has partnered with Xiphera to deliver quantum-safe cryptographic capability on iWave’s Agilex™ 5 System on Module (SoM) powered by Altera.
How to Select Cables for Reliable VFD Motor Control and Sensor Feedback
Publish Date: 2026-03-24
Growing industrial automation and the push for better energy efficiency are speeding up the adoption of VFDs in motor-driven systems.
Solder Smarter Using DigiKey Standard Helping Hands
Explore DigiKey Helping Hands features including magnetic PCB pillars, flexible arms, LED magnifier, and a heavy steel base for stable soldering.
Automotive Ethernet: The Backbone of Modern In-Vehicle Communication
As vehicles become more autonomous and data-centric, the need for a high-speed, scalable, and reliable in-vehicle communication backbone is greater than ever.
Webinar – Select the Right Cables for Harsh Industrial Automation Applications
This in-depth webinar breaks down what it takes to select the right wire and cable for industrial environments.
Pushing the Limits: A 6km LoRa Range Test with the PTSolns SX1276 Shield
In this blog, we’ll explore the hardware that’s being used, the science behind the transmission, and just how impressive a feat it is to achieve a 6km range.
How Hardware Gets Hacked (Part 2): On-boarding
Explore a hardware security workflow using firmware builds, simulation tools, serial commands, and automated tests for microcontroller systems.
Detecting High-Impedance Ground Faults: Limitations of Standard GFDI and Active Diagnostic Solutions
Publish Date: 2026-03-18
An examination of the limitations of standard GFDI, the physics of high-impedance faults, and the practical challenges of locating them in 1500 V arrays.
Criteria for Cable and Wire Selection
Publish Date: 2026-03-17
Cable design needs to focus on the system concept, integrating the installation method, electrical and mechanical loads, as well as cost-effectiveness.
Why We Need New Op Amps Despite Already Having So Many Good Ones
Older op amps offer designers confidence, while new ones offer vendors the potential for long-term bill-of-materials winners.
How to Overcome Linux Development Hurdles in Resource-Constrained Systems
Publish Date: 2026-03-12
Learn how the BeagleBoard.org BeagleV-Fire single-board computer addresses common hurdles for running Linux in resource-constrained systems.